This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS3300: Is it possible to use IO link(COM3) of 230.4kbps

Part Number: TVS3300


Dear Specialists,

My customer is considering TVS3300 and has a question.

Could you please advise?

---question---

According to the datasheet, it can use for IO link.

Is it possible to use IO link (COM3) which is specified 230.4kbps?

The device has a capacitance 130pF, are there any problem? 

---

I appreciate your great help in advance.

Best regards,

Shinichi