This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux xHCI driver for TUSB73x0



Dear Sir,

May I know where can get this driver for non-Windows O/S ?

TKS!

 

  • Terry,

    It is also supported in Linux in the open source community, The latest supported Linux releases of 2.6.32 onward all have xHCI support, it just needs to enabled in the kernel configuration.  Whatever is one's current source for Linux, that is where to go for the xHCI driver. Support has been there since 2.6.31 (2.6.31 is in no way recommended, xHCI support was not all robust initially).  Here are the kernel versions I recommend based on when kernel.org went offline.
          3.0.4 -- most robust
          2.6.39.4
          2.6.35.14 -- stable, will work with our host, but won't be as robust
          2.6.32.46 -- stable, will work with our host, but won't be as robust
    To get the most out of TI's controller, using the newest possible kernel version is recommended. While the latest 2.6.32.x through 2.6.35.x are supported, I recommend going with a newer kernel release, preferably the latest 3.x stable release.

  • I saw this email after I opened one thread on the same topic. I am trying to use 73xx on FC15 running kernel 3.0.4, but when I insert the driver, I see a kernel crash. Any idea ?

  • Have you tried 3.0.17? 3.0.4 is no longer supported. http://www.kernel.org/ has the list of stable kernels contain TUSB73xx support with the xHCI driver.