Hi,
1, Here is a MDIO application to support live insertion. In below circuits (Modified from datasheet Figure 9), there is a 2.5V MDIO Master in left side. For live insertion sub cards at righ side, some sub cards are 3.3V MDIO, others sub card are 2.5V MDIO. Does it work at 15Mbps?
2, If I'd like to support both side 3.3V MDIO, set Vref_A=3.3V, Vref_B & EN 200kOhm to 5V, Vpu=3.3V, does it work?
I saw Voltage-Level Translation With the LSF Family (Rev. B) . Hope get your comfirmation. Thanks.
Best Regards,
Shawn