Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848 and STM32F407VET6 no communication.

I have the subjes mounted on my development board for academic project.

I use interface RMII. 50 Mhz clk goes from PA8 pin. (PLL_CLK=100MHz / 2). Xtal is 25 MHz 20 pf CL and 30 ppm. The clocking seems to be stable.

Schematic are typical for RMII and other parts too. RESET and POWER_DOWN pins are at 3.3V. I checked soldering and schematic but no issues were detected by me.

And each time when I had tried to execute something like

temp = ETH_ReadPHYRegister(0x01, 0x02);

I got only 0x0000FFFF.

Note. There is no clocking at 25 pin.

Oscilloscope shows me the STM32F407VET6 toggles MDC and MCIO lines, but DP83848CVV does not responding. I saw only 3.3V level (that means 0x1111).

How to check if the IC was not damaged?

Help, please. I gave up the attempt in despair.