I am new to this forum and have browsed somewhat through it on this subject, but have not found a solution that helps me, so I thought I'd post. I am an analytical chemist working on a project to design a handheld instrument which contains an embedded CPU board and an LCD panel. The LCD panel we selected for the application has an LVDS interface (24-pins, some of which are for the LED back light). The embedded CPU board we have chosen does not have a native LVDS output (I can get one with the addition of a bulky expansion board), but it does have an HDMI output.
The supplier of the panel provided me with a large (8.5" x 3") board that uses a chip (RTD2662, from RMC) that is used to provide a wide range of video connectors (HDMI, DVI, SVideo) for inputs and it drives the particular panel we have been testing via a custom cable the integrator provided. We were able to drive the panel as a second monitor via the HDMI output of a PC. Thus, I know it can be done.
However, we are very space limited in our design, and this board is much too large for us, and is overkill. I only need one HDMI input and the ouptut to go to the LVDS input of the panel. I am looking for help to understand what this will take.
Ideally, given our short development cycle, I would like to find a very small COTS circuit that would do this for me. If that does not exist, then suggestions for the fastest route to a solution.
Any help would be appreciated.