This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q I2S_CLK frequency



DS90UB925Q datasheet (SNLS407C) describes : "The bit rates of any I2S bits must maintain one fourth of the PCLK rate". Does this mean if PCLK is 32MHz the I2S_CLK frequency must be 8MHz?

On the one hand, FPD-Link III application note (SNLA221) describes : "I2S_CLK frequency for DS90Ux92x devices must be maintained below PCLK/2 or 12.288MHz, whichever is lower."

For DS90UB925Q, can the I2S_CLK frequency be lower than PCLK/4? If PCLK is 32MHz can the I2S_CLK frequency be 1.411MHz?

Best regards,

Daisuke