This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Logic maximum speed



hello,

I want to use a 74AUP1G125 as a buffer for a 15MHz clock signal. I have seen in the datasheet :

   Δt/Δv Input transition rise or fall rate VCC = 0.8 V to 3.6 V    200 ns/V

Does it mean that the maximum frequency, if Vcc=3.3V, is 757KHz?

This is  200ns/V * 3.3V *2(rise+fall)= 1320ns ==> 757KHz