This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

code compilation showing errors

Other Parts Discussed in Thread: Z-STACK

Hi all,

I am using zstack home 1.1.0 and trial version of IAR WB 8.20

i am getting a lot of errors while compiling the code. the same code works fine the previous evening and next day morning, i see a lot of errors.

today i installed IAR WB 8.3 trial version.  and now i find that the previously working code ( compiled with v8.20) is giving me the following errors.  

""Error[e46]: Undefined external "?V12" referred in AF ( E:\BetaBackup - heartBeat\ZC_bc_7_SWStatusAtRestart_Redo\   ""

did anyone got these type of errors earlier?

why am i getting these errors? this is a compiled and working code till morning. now i am getting these type of errors from ?V1 to ?V15.

Pl. help me in solving these errors.  i compared the project options of both IAR v8.2 and v8.3.  they are same. then what could be the problem?

Thanks in advance ,

Mahesh KV