Hi all,
we are finding that with the Mistral AM37xx EVM, LSR WL1271 daughtercard and latest SDK 6.00.00.00
http://downloads.ti.com/sitara_linux/esd/AM37xSDK/latest/index_FDS.html
we are starting the SoftAP via the matrix app and it starts up and puts out the right SSID, but somehow we cannot associate with it. The driver firmware is
root@am37x-evm:~# [ 93.678100] wl12xx: state: 0
[ 94.221282] wl12xx: firmware booted (Rev 6.3.10.0.135)
[ 94.301666] wl12xx: removing interface 00:00:00:00:00:01
[ 94.309967] wl12xx: state: 0
[ 94.775970] wl12xx: firmware booted (Rev 6.3.10.0.135)
wlan0 Link encap:Ethernet HWaddr 00:00:00:00:00:01
inet addr:192.168.0.1 Bcast:192.168.0.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Have we tested this?
Thanks,
--Gunter