This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: ADC Pins That Have Internal Capacitors or Resistors Which Cannot be Disabled - What is the Expected Tolerance?

Part Number: TMS320F28075


The TMS320F28075 datasheet shows that the following dual use pins (ADC or Other function) have internal resistors or caps that are present regardless of pin mode (i.e. being used as ADC input).

ADCINA0 / DACOUTA - 50kOhm

ADCINA1 / DACOUTB - 50kOhm

ADCINB0 / VDAC - 100pF

ADCINB1 / DACOUTC - 50kOhm

Customer needs to know the tolerance of these internal resistors and capacitors for proper design analysis.

Please advise.

Kind Regards,

-Marc