I've been circling the RM42 TRM (SPNU596A) sec 17.2.5.3/.4 and the Forum, and I haven't been able to answer this.
Can I use the N2HET to perform input capture on multiple (e.g. 4x) separate pins in High Resolution?
For each pin, the input frequency is fairly low (a few kHz), but I need high precision (at least 16MHz) in the captured timestamps, and I need them to have the same timebase (i.e. comparable to one another). The inputs are not correlated, so it is entirely possible that more than one pin will have a (single) edge within a single LRP.
There's nothing exotic here -- this is something done routinely with "traditional" timers (given 4x CCRs and a fast-enough clock).
What I've read seems to wander between "one HR capture per LRP" and "one HR capture per pin per LRP", where the distinction between these two is critical for my purposes.