Hello all,
I a student and working on a project.
The project is very low power circuit.
I am having a problem with interfacing with AT86RF231.
First I will describe a little bit what I am doing.
The input of the circuit is 0.8 V. Then I have installed the rectifier so that I can use dual polarity at the input.
The 0.8 V is increased to 4 Volts by booster.
The 4 V is divided here. One lead goes to the voltage regulator (Max8880) to constant it to 2.7 V. This Voltage power up all the ICs in the Board.
The 4V is also connected to the Super Capacitor to charge it and the charging start according to the programming in MSP430.
Now the Problem is If i turn on the power and increase it to 0.8 V the output stuck at 1.8 V.
If I hold the push button attached to the reset pin of the MSP430 the output voltage start increasing and then reach the 2.7 V at that point if I release the push button the voltage stays at 2.7 V and RF starts working.
And also some time when the output reaches 2.7 V the RF doesnot work and then if i press the reset button it starts working.
I also attached the reset rising edge image in the post.
I try to put the voltage supervisor in the program but it doesn't work out at all. As I put the threshold to 2.5 V the output voltage then stays all the time at 2.5 V and donot increase.
Does anybody have any hint about it...???
Thank you in advance
Regards
Sarmad