Hello,
We recently purchased the new msp-fet debugger/programmer device as we discovered the msp-fet30uif was being discontinued. However, I am now running into quite a few problems trying to get the new device to work.
I am using Code Composer Studio V 5.4.0.00091. When i try to load my program onto a board, an error pops up that there is no device available.
I also use Elprotronics Fet-Pro430 Lite, and that as well is having issues, flashing an error that the msp430.dll has trouble initializing. So i upgraded to the latest Fet-Pro430 Lite (V3.3), and while I don't get the .dll error with the new msp-fet, now NEITHER the msp-fet nor the msp-fet430uif will load code or read memory, each of which fails at verifying the security fuse.
Has anybody made the switch from the msp-fet430uif to the msp-fet, and/or can anyone provide any insight as to what could possibly be my problem?
Thanks in advance!