This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

microcontroller programming



Hi, 

I am trying to program the CC22541 based bluetooth module from LSR.  http://www.lsr.com/downloads/products/330-0134.pdf

I am using CC Debugger and Free Evaluation version of "IAR Work bench for 8051".  I am trying to program the CC22541  to work with UART protocols so that I can interface it with MSP430F5438A's UART (Txd and RxD). 

I downloaded the "SimpleBLEPeripheral_UART" files from the TI website processors.wiki.ti.com/.../CC254X_WITH_EXT_MCU

The problem is that I am unable to compile the code , download and debug it . 

Have someone worked on this issue before ? I am getting the following error 

[Su007]: Unable to open the command file "C:\Program Files\IAR Systems\ElectroCore Project\SimpleBLEPeripheral_UART patch\Projects\ble\

jess

  • Another E2Eer posted an almost identical request.
    e2e.ti.com/.../398592
  • okay. whats ur point fat cow
  • I guess he wants to point out that it is pointless to ask the same question in a different thread. If another thread covers the same question, either your answer is already there, or you will not get an answer too in your thread. In any case, it is better add your request to an existing thread with the same topic than creating your own. LAso, your thread title is as generic as "help" or "I have a problem" would have been: not attracting anyone to bother reading it.
    Now this other thread doesn't exactly cover the same question, but the answer is basically the same:

    This question is about IAR compiler and 8051 and CC22541, and this forum is about Ti and MSP430 processors. So it would be pure coincidence if you'll find someone here who can give you an answer.

    However, one general suggestion: check the access rights to the given path. The project seems to be below the program installation path, where a running application normally has no write permissions since Vista. Written data is usually redirected to c:\ProgramData\... but this may cause problems with more complex access situations, especially when using console-based tools like make,as used for most compilers.
    Don't install your projects in/below the program folder.
  • WTF?! Fat cow?

**Attention** This is a public forum