Other Parts Discussed in Thread: CC3200, MSP430FR5994
I recommend that TI seriously consider adding native I2S support in future revisions of the MSP432.
I know about this: "SLAA449A– Interfacing an I2S Device to an MSP430 Device"
But is clear from follow-on threads, that while it is possible now to use a SPI port to create such an interface, the software required is very cumbersome.
With the availability of Class D amplifiers with I2S interfaces, it would be great to be able to use those Class D amplifiers without first converting to analog.
These amplifiers are useful for generating low-frequency signals, which could potentially be signals that are not audio. I have such an application now; my load is inductive, but otherwise is unrelated to audio.