This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: I2C setting MCU as both slave and master at the same time

Part Number: MSP432P401R


Hello everyone I'm working on a new project with the TI MSP432P401R microcontroller. I want to have 2 separate I2C buses. I2C bus 1 will set the MCU as the master, whereas the DAC and the pressure sensor as slaves. Then I2C bus 2 will set the same MCU as the slave, and the SmartPort as the master (more specifically a device that we connect to the SmartPort will be the master). I'm not sure how can I make the MCU both a slave and a master at the same time. What I tried to do was, I defined 2 different eUSCI_b modules

void I2C_init(void)
{
/* Initialize USCI_B3 and I2C Master to communicate with slave devices*/
I2C_initMaster(EUSCI_B3_BASE, &i2cConfig);

/* Disable I2C module to make changes */
I2C_disableModule(EUSCI_B3_BASE);

/* Enable I2C Module to start operations */
I2C_enableModule(EUSCI_B3_BASE);

/* Initialize USCI_B3 and I2C Master to communicate with slave devices*/
I2C_initMaster(EUSCI_B0_BASE, &i2cConfig);

/* Disable I2C module to make changes */
I2C_disableModule(EUSCI_B0_BASE);

/* Enable I2C Module to start operations */
I2C_enableModule(EUSCI_B0_BASE);

return;
}

//where i2cConfig is

const eUSCI_I2C_MasterConfig i2cConfig =
{
EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
48000000, // SMCLK = 48MHz
EUSCI_B_I2C_SET_DATA_RATE_400KBPS, // Desired I2C Clock of 100khz
0, // No byte counter threshold
EUSCI_B_I2C_NO_AUTO_STOP // No Autostop
};

and then tried to use this function for each module I defined to add slaves. But the thing is, the function only allows me to enter one slave address, but for my I2C bus1, I have 2 slaves: DAC and the pressure sensor.

extern void I2C_initSlave(uint32_t moduleInstance, uint_fast16_t slaveAddress,
uint_fast8_t slaveAddressOffset, uint32_t slaveOwnAddressEnable);

I would be very grateful if someone can help me with this problem or show me a better way to implement the same MCU as both a slave and a master at the same time. I'm new to programming with the I2C protocol and I'd appreciate any help. Thank you and have a great day.

**Attention** This is a public forum