We're glad to announce that we've just released the MSP430.DLLv3 - TI's all new MSP430 Debug Stack!
The MSP430.DLLv3 is the component in between your IDE and the MSP430 microcontrollers when you download or debug code. This all new version provides faster debugging and significant stability improvements. In addition, it is available as OPEN SOURCE and was created in an host operating independent manner!
The first product that includes the new MSP430 debug stack is CCSv5.1, the IAR Embedded Workbench and all other 3rd party product releases will follow immediately. The migration to the new MSP430.DLLv3 works in a fully automated manner (see important note below).
The MSP Debug Stack Wiki page www.ti.com/mspds contains all information and download links.
YOUR FEEDBACK COUNTS!
We're highly interested in any feedback! Please use the E2E forum to provide feedback or to contact us in case problems.
IMPORTANT NOTE:
(1) This software requires an update of the MSP-FET430UIF firmware that goes beyond the usual updates. In addition to the firmware, also the USB stack of the debugger will be updated. Once an update was done, the debugger won't work with old IDE versions ("Interface not found"). However, CCSv5.1 includes a small utility that allows downgrading the debugger at any time to be used with old IDE versions and utilities again. Please see www.ti.com/mspds.
(2) Old MSP-FET430UIF interfaces may require an extra step in the automated update procedure. Please visit www.ti.com/mspds for additional information.