Hey People,We are Making a face recognition system for our final year project and we have developed the Fully working software in MATLAB.We are able to get output with and accuracy of 97% in MATLAB.
Also we have converted our code to C using Embedded coder.
We require about 128 MB of space for storing all the program and variables (eigenfaces,images and output variables)
Now we are using MSP430.Is it possible to interface a 128 MB ram with MSP430?
Also we have a DSK6713 board in our college.We can use that.We are confused due to large memory requirement.
So i have following questions:
1) Can we interface 128 MB RAM(Flash or any memory) with MSP430.(We have purchased Launchpad)
2) Also If that is not possible then is it possible to have AN EXTERNAL CODE MEMORY for DSK6713?
Plz give us a solution to our problem.
-Mehul Saxena