I am using the MSP430F5529.
Section 3.7 of http://www.ti.com/lit/ug/slau319b/slau319b.pdf says that if I execute the instruction at 0x1000 then I will just “happen” to execute the instruction to jump to the BSL. My concern is that with only the RXD and TXD connected to the PC UART will my newly designed BSL still see the BSL commands from the PC without the other required pins hooked up (in particular DTS to Reset control and RTS to TEST)? (See SLAU319b section 4.1.2) This scheme worked on the F149, will it still work?
Cheers
Calum