This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 5529 Rev A enumeration fails (USB)



Hi,

I am having problems with the USB enumeration on the MSP430 5529 Rev A.
I am using the CDC API from TI with Code Composer Studio Core 4.2.1.00004 and a TS430PN80USB Board.

The microcontroller will go into ST_ENUM_IN_PROGRESS, when I start it and stays there.

The virtual com port is showing up in the windows device manager and the driver is installed.

The HID example does go into the ST_ENUM_ACTIVE state, but I have to get the CDC examples to work.

**Attention** This is a public forum