My MSP430 LaunchPad is working correctly (of course the red and green LEDs are reversed from the video example). If I connect to COM15 (the USB serial port) with Hyperterminal (2400 baud) I see single characters that appear to start with '?' or '@' and then proceed to the alphabetic characters 'A', 'B', 'C', etc. as the temperature increases and then back down in value as the temperature decreases. However, the GUI only puts up a screen showing my two serial ports and COM15, the MSP serial port, but there is no way to select the COM15. Mouse clicks do not work nor does entering a 2 (third port listed) or COM15. What is the secret of selecting the desired port?