This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: JTAG connection

Part Number: TM4C1294NCPDT


Hi,

I am going to design my own PCB board using TM4C1294NCPDT controller. I have gone through system design guidelines for TM4C129x and TM4C12x Devices Over JTAG Interface for JTAG connection.I am choosing cortex ARM 10pin debug connector. When this micro controller has default internal pull up resistor for TCK, TMS, TDI and TDO means whether this connection is sufficient for JTAG connection.   

  • Those internal, MCU resistors are (very) high in value.   (~50K+)

    While they (have) worked - the signal edges & potential for signal reflection - renders them,  "sub-optimal."     Our firm has found - over many years - that external resistors (~10K) - installed very close to the MCU's JTAG/SWD pins - prove FAR more robust.

    Should you employ the Forum Search Box (atop this page) - you will note (many) difficulties in establishing JTAG connection.     Often - such is noted via the (saving) of those,  "enhanced signaling,"  external resistors...     Risk-Reward (strongly) argues for their deployment...

  • Hi Nishitha,
    Cb1 is correct. Please add the external pullup resistors as shown in the guideline for proper operations.
  • Hi Sir,

    Sorry, I have a doubt what about that R13,R14, R15 and R16 - 33ohm resistor. Whether it is required or not ??

  • Squelch you doubt - those resistors provide a useful, "Safety Factor" - protecting the critical JTAG inputs from (reasonable) transients - while reducing the impact of "noise."    The "cost/size" adder of 4 smt resistors makes their implementation a "No brainer."

    Client-users must ALWAYS "factor in" the costs of  "Board Failure" - and/or  "Difficulty in JTAG Programming/Debug" - which (unfortunately) is NOT "unknown" here...     Those resistors ADD robustness - case closed!