Hello !
I have a problem about the hibernate of Tiva MCU. The code is put below.
SysCtlPeriEnable(SYSCTL_PERIPH_HIBERNATE);
SysCtlDelay(2 *(12000000UL));
HibernateEnableExpClk(SysCtlClockGet());
SysCtlDelay(25 *(12000000UL / 1000));
HibRTCSet(35920UL);
SysCtlDelay(50 *(12000000UL / 1000));
HibRTCEnable();
When the code gets into HibernateEnableExpClk(SysCtlClockGet()),it stops. If I remove HibernateEnableExpClk(SysCtlClockGet()) , the program can work continue,but the RTC can't get initial value. The crystal of the hibernate is 32.768KHz. When I use oscilloscope to watch the cystal, the input voltage of the crystal is -0.1mv -0.1mv ,the frequency is 32.768KHz, but I can't get the output of the crystal. The value of HIB_CTL_WRC is always 1.Why the HibernateEnableExpClk(SysCtlClockGet()) can't work , thank you for your reply!