This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva C CAN bit Timing error



 Hi, Ti employed.

 If  the Tiva series still implements the Bosch C_CAN module, I think that there are several error in Tiva C ware CAN driver.

typedef struct
{
    //
    //! This value holds the sum of the Synchronization, Propagation, and Phase
    //! Buffer 1 segments, measured in time quanta.  The valid values for this
    //! setting range from 2 to 16.
    //
    uint32_t ui32SyncPropPhase1Seg;  

    //
    //! This value holds the Phase Buffer 2 segment in time quanta.  The valid
    //! values for this setting range from 1 to 8.
    //
    uint32_t ui32Phase2Seg;

    //
    //! This value holds the Resynchronization Jump Width in time quanta.  The
    //! valid values for this setting range from 1 to 4.
    //
    uint32_t ui32SJW;

    //
    //! This value holds the CAN_CLK divider used to determine time quanta.
    //! The valid values for this setting range from 1 to 1023.
    //
    uint32_t ui32QuantumPrescaler;
}
tCANBitClkParms;

The source code CANBitTimingGet() shows  psClkParms->ui32SyncPropPhase1Seg = ((ui32BitReg & CAN_BIT_TSEG1_M) >> CAN_BIT_TSEG1_S) + 1;

This means that ui32SyncPropPhase1Seg => CAN_BIT_TSEG1_S = Prop + Phase1Seg,  it does't include Sync.

As a result,  CANBitTimingSet() function incorrectly set the can bit timing parameter.  

For Example, 

    SystemClock : 80Mhz, BitRate: 500 kbps

    CANBitRateSet(CAN0_BASE, 80000000, 500000); 

    CANBitTimingGet(CAN0_BASE, &g_sCANBitClkParms);

This code set the  g_sCANBitClkParms as follows.

g_sCANBitClkParms ->ui32SyncPropPhase1Seg = 8

g_sCANBitClkParms->ui32Phase2Seg = 6

g_sCANBitClkParms->ui32QuantumPrescaler = 9

These are real value( resister value + 1 ).

#define CAN_BIT_VALUE(seg1, seg2, sjw)                                        \
                                ((((seg1 - 1) << CAN_BIT_TSEG1_S) &           \
                                  CAN_BIT_TSEG1_M) |                          \
                                 (((seg2 - 1) << CAN_BIT_TSEG2_S) &           \
                                  CAN_BIT_TSEG2_M) |                          \
                                 (((sjw - 1) << CAN_BIT_SJW_S) &              \
                                  CAN_BIT_SJW_M))

static const uint16_t g_ui16CANBitValues[] =
{
    CAN_BIT_VALUE(2, 1, 1),     // 4 clocks/bit
    CAN_BIT_VALUE(3, 1, 1),     // 5 clocks/bit
    CAN_BIT_VALUE(3, 2, 2),     // 6 clocks/bit
    CAN_BIT_VALUE(4, 2, 2),     // 7 clocks/bit
    CAN_BIT_VALUE(4, 3, 3),     // 8 clocks/bit
    CAN_BIT_VALUE(5, 3, 3),     // 9 clocks/bit
    CAN_BIT_VALUE(5, 4, 4),     // 10 clocks/bit
    CAN_BIT_VALUE(6, 4, 4),     // 11 clocks/bit
    CAN_BIT_VALUE(6, 5, 4),     // 12 clocks/bit
    CAN_BIT_VALUE(7, 5, 4),     // 13 clocks/bit
    CAN_BIT_VALUE(7, 6, 4),     // 14 clocks/bit
    CAN_BIT_VALUE(8, 6, 4),     // 15 clocks/bit
    CAN_BIT_VALUE(8, 7, 4),     // 16 clocks/bit
    CAN_BIT_VALUE(9, 7, 4),     // 17 clocks/bit
    CAN_BIT_VALUE(9, 8, 4),     // 18 clocks/bit
    CAN_BIT_VALUE(10, 8, 4)     // 19 clocks/bit
};

if Sync+ Prop +Phase1Seg = 8  and  Phase2Seg = 6, Total Tq(Time quanta) = 14. 

In this case,  the ui32QuantumPrescaler must have non-integer value or bit rate is not 500kbps.

if Prop +Phase1Seg = 8, Sync =1 and  Phase2Seg = 6, Total Tq = 15.

In this case, the ui32QuantumPrescaler should have 11.

I think that there are mutual error in the CAN divice driver bit timing sourcecode and document.

Please check!