hi,
I install android GB from prebuild binaries, bt wlan, camera is not working for Blaze.
need hlp.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
I install android GB from prebuild binaries, bt wlan, camera is not working for Blaze.
need hlp.
Hello Soumya,
What specific release are you using for the GB prebuilt binaries?
The probable reasons for the wlan and camera not working are missing firmware.bin and ducati binaries, respectively.
Check your system/etc/wifi/ and see if firmware.bin is present. If not, simply follow the instructions at the end of the release notes (the link is for G3 as an example): http://www.omappedia.org/wiki/L27.G.3_OMAP4_GingerBread_Release_Notes. Also make sure to undergo the WLAN calibration steps to optimize wifi performance.
As for the ducati binaries, they are not included with public prebuilt binaries. if working with GB releases, you need to contact your local TI representative for them.
Alternatively, if you decide to use IS releases, http://omappedia.org/wiki/4AI.1.2_OMAP4_Icecream_Sandwich_Release_Notes, the firmware and ducati binaries come included with the repo sync.
Regards,
Alex Trinh