Hi Ti
I'm about to design a current fed full-bridge converter
Specs:
Vin: 27V - 42V
Iin: 13A
Vout: 300V - 600V
What i need is a pwm controller that is able to go above 50% duty cycle on all switches.
The schematic is as follows.
I have looked at the LM5045, would this IC be suitable?
I'm curious as there is no description of a inductor on the input side, or mentioning of duty cycles above 50%.
If there is a more suitable IC, i would be happy to know.
Best regards
Kristian K