With the 3 boards: base, daughter and LCD board stacked up, and with sysboot[4:0] set to 00001b, I could see "CCCC.." appear on my TeraTerm screen when the system is powered up, the system then proceed to boot from SDCard without any problem.
But when I removed the daughter board and LCD board, powered up the base board, nothing appear on my TeraTerm screen.
Is it because the CPU does not boot at all ?
What are the signals needed from the daughter board to the base board in order for the baseboard to boot ?
And what kind of rework needed in order to boot up the base board without the daughter and LCD board ?