Hi,
We are trying to enable OTG micro USB on the am335x and we have selected the below mentioned changes in the menu config.
In Device Drivers We have selected USB support and in that the below mentioned are selected as shown below:
[*] USB support  --->     
    <*>   Support for Host-side USB                                        
    [ ]     USB verbose debug messages                                     
    [*]     USB announce new devices                                       
    *** Miscellaneous USB options ***                              
    [*]     USB device filesystem (DEPRECATED)                             
    [*]     USB device class-devices (DEPRECATED)                          
    [*]     Dynamic USB minor allocation                                   
    [*]     USB runtime power management (autosuspend) and wakeup          
    [*]       OTG support    
    [*]   Rely on OTG Targeted Peripherals List                            
    [ ]   Disable external hubs                                            
    <*>   DesignWare USB3 DRD Core Support                                 
    [ ]     Enable Debugging Messages                                      
    <*>   USB Monitor        
    -*-   Enable Wireless USB extensions (EXPERIMENTAL)                    
    <*>   Support WUSB Cable Based Association (CBA)                       
    [*]     Enable CBA debug messages                                      
    *** USB Host Controller Drivers ***                              
    < >   Cypress C67x00 HCD support                                       
    <*>   EHCI HCD (USB 2.0) support                                       
    [*]     Root Hub Transaction Translators      
    [*]     Improved Transaction Translator scheduling                     
    [*]   EHCI support for OMAP3 and later chips                           
    < >   OXU210HP HCD support                                             
    < >   ISP116X HCD support
    < >   ISP 1760 HCD support                                             
    < >   ISP1362 HCD support
    <*>   OHCI HCD support   
    [*]     OHCI support for OMAP1/2 chips                                 
    [*]     OHCI support for OMAP3 and later chips                         
    < >   SL811HS HCD support
    < >   R8A66597 HCD support                                             
    <*>   Host Wire Adapter (HWA) driver (EXPERIMENTAL)                    
    <*>   Inventra Highspeed Dual Role Controller (TI, ADI, ...)           
        *** Platform Glue Layer ***                                    
    < >     TUSB6010         
    < >     OMAP2430 and onwards                                           
    < >     AM35x            
    <*>     TI81XX onward    
    [*]     Disable DMA (always use PIO)                                   
    < >   Renesas USBHS controller   
      *** USB Device Class drivers ***                                 
    < >   USB Modem (CDC ACM) support                                      
    < >   USB Printer support
    <*>   USB Wireless Device Management support                           
    <*>   USB Test and Measurement Class support                           
          *** NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may ***     
          *** also be needed; see USB_STORAGE Help for more info ***       
    <*>   USB Mass Storage support                                         
    [ ]     USB Mass Storage verbose debug                                 
    < >     Realtek Card Reader support                                    
    < >     Datafab Compact Flash Reader support                           
    < >     Freecom USB/ATAPI Bridge support                               
    < >     ISD-200 USB/ATA Bridge support                                 
    < >     USBAT/USBAT02-based storage support                            
    < >     SanDisk SDDR-09 (and other SmartMedia, including DPCM) support 
    < >     SanDisk SDDR-55 SmartMedia support                             
    < >     Lexar Jumpshot Compact Flash Reader                            
    < >     Olympus MAUSB-10/Fuji DPC-R1 support       
    < >     Support OneTouch Button on Maxtor Hard Drives                  
    < >     Support for Rio Karma music player                             
    < >     SAT emulation on Cypress USB/ATA Bridge with ATACB             
    < >     USB ENE card reader support                                    
    <*>   USB Attached SCSI  
    [ ]   The shared table of common (or usual) storage devices            
          *** USB Imaging devices ***                                      
    < >   USB Mustek MDC800 Digital Camera support                         
    < >   Microtek X6USB scanner support                                   
          *** USB port drivers ***                                         
    <*>   USB Serial Converter support  --->                               
          *** USB Miscellaneous drivers ***                                
    < >   EMI 6|2m USB Audio interface support                             
    < >   EMI 2|6 USB Audio interface support                              
    < >   ADU devices from Ontrak Control Systems                          
    < >   USB 7-Segment LED Display                                        
    < >   USB Diamond Rio500 support                                       
    < >   USB Lego Infrared Tower support                                  
    < >   USB LCD driver support                                           
    < >   USB LED driver support                                           
    < >   Cypress CY7C63xxx USB driver support       
       
    < >   Cypress USB thermometer driver support                           
    < >   Siemens ID USB Mouse Fingerprint sensor support                  
    < >   Elan PCMCIA CardBus Adapter USB Client                           
    < >   Apple Cinema Display support                                     
    < >   USB 2.0 SVGA dongle support (Net2280/SiS315)                     
    < >   USB LD driver      
    < >   PlayStation 2 Trance Vibrator driver support                     
    < >   IO Warrior driver support                                        
    < >   USB testing driver 
    <*>   USB OTG & EH Test Mode Support driver                            
    < >   iSight firmware loading support                                  
    < >   USB YUREX driver support                                         
    <*>   USB Gadget Support  --->                                         
          *** OTG and related infrastructure ***                           
    <*>   GPIO based peripheral-only VBUS sensing 'transceiver'            
    < >   Philips ISP1301 with OMAP OTG                                    
    [*]   Generic ULPI Transceiver Driver                                  
    <*>   TWL6030 USB Transceiver Driver                                   
    -*-   NOP USB Transceiver Driver                   
                
 --- USB Gadget Support   
[ ]   Debugging information files (DEVELOPMENT)                        
[ ]   Debugging information files in debugfs (DEVELOPMENT)             
(2)   Maximum VBUS Power usage (2-500 mA)                              
(2)   Number of storage pipeline buffers                               
<M>   USB Peripheral Controller                                        
< >     Faraday FUSB300 USB Peripheral Controller                      
< >     OMAP USB Device Controller                                     
< >     Renesas R8A66597 USB Peripheral Controller                     
< >     DesignWare USB3.0 (DRD) Controller                             
< >     Inventra HDRC USB Peripheral (TI, ADI, ...)                    
< >     Renesas M66592 USB Peripheral Controller                       
< >     PLX NET2272      
< >     Dummy HCD (DEVELOPMENT)                                        
<*>   USB Gadget Drivers (Gadget Zero (DEVELOPMENT))  --->             
        Gadget Zero (DEVELOPMENT)                                      
[ ]       HNP Test Device   
I am getting the following error when I plug in SDcard reader.
root@am335x-evm:~# [  727.161437] usb 2-1: new high-speed USB device number 11 using musb-hdrc
[  727.315704] usb 2-1: device v05e3 p0723 is not supported
[  727.321289] hub 2-0:1.0: unable to enumerate USB device on port 1
I can see that AM335X_USB0_DRVVBUS is driven low. How to make this pin logic high.
Please suggest me how to resolve this error and teach me how to make AM335X_USB0_DRVVBUS logic high.
Regards,
Ajith