Hi everyone,
Some weeks ago, we tested Spansion S34ML02G100TFI000 with success using u-boot. We could read, write and boot from that flash. Since that NAND will be EOL later this year we want to switch to the successor S34ML02G200TFI000. And now we have problems booting from that NAND.
Writing (and reading) the u-boot bootloader works as expected. But the board just won't boot from it.
The data sheet mentions two main differences:
S34ML02G100TFI000: "64byte spare area" and "1-bit ECC" (ONFI Parameter Page, Byte 112 => 01h)
S34ML02G200TFI000: "128byte spare area" and "4-bit ECC" (ONFI Parameter Page, Byte 112 => 04h)
So, does anyone have any idea, why the boards RBL won't boot from the new NAND?
Greetings,
Thomas