Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thermistor circuit design based on reference sloa052 and sboa097

Other Parts Discussed in Thread: REF200, LM335, INA330

I have designed my NTC Thermistor circuit based on reference sloa052 and sboa097.

But the input temperature range is from -40C to +150C instead of from 0C to +100C.

When input temperature is -40C, the resistance of Thermistor is 191908 ohm, which means the input voltage will be +20V if I use REF200.

I have selected Circuit 2: Single-Supply/Single-Part Approach in sboa097 to reduce the input voltage down to +3.3V ADC interface.

Please send me any suggestions if my idea is practical.

Many thanks.