I'm evaluating the TDC1000-TDC7200EVM roadtest at element14.
The module and GUI work fine. I do have one issue though:
When I generate a new Register file in Webench
I used Max fluid level 0.5 m, min fluid level 0.01m, Accuracy 3mm, Automotive Q -grade needed false, speed of sound 1480 (water), sensor SMD15T21R111WL.
I get errors when importing in the GUI's TDC1000 tab (firmware 2.01, GUI Revision 1.2.7.1). The kit doesn't sample after I've loaded that registry file in registry.
I've attached a zip with the downloaded registry file and the export of the settings after loading that file (as advised by the error dialog)
fyi, link to my roadtest articles: