Other Parts Discussed in Thread: DCA1000EVM
Hi,
My customer is using IWR1642 and have below questions about DCA1000 EVM. Would you pls help?
1. Can DCA1000 EVM work without Radar studio?
Customer would like to power on the DCA1000 EVM and use own PC software to capture the radar data on Ethernet port. Radar chip config can be hard coded in customer's software. I found there is hardware switch configuration mode for DCA1000EVM. So this is supported, right?
2. Can DCA1000 EVM support to capture the radar raw data with sub-frame configure (e.g. 4 sub frames in one frame, with different number of ADC sample, different number of chirps in each sub frame)?
3. Can customer use IWR1642 and DCA1000 to capture the radar data which is beyond the capability of IWR1642 to process on DSP/MCU? For example, if IWR1642 can't process one certain frame config (e.g. 256 chirps with 512 ADC sample), can customer disabled the radar data process on DSP/MCU and only output radar on LVDS, then DCA1000 EVM to capture the radar data for some research?
I think if the radar raw data throughput with customer's config is less than xwr1642 LVDS interface own max throughput, this can be supported. Would you pls help to confirm?
4. What's the max throughput on Ethernet TI has ever tested with DCA1000 EVM?