This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

AWR1243: Cascade option not supported in all AWR1243 chips

Prodigy 70 points

Replies: 7

Views: 196

Part Number: AWR1243

HI:

I have two questions.

(1) We are using the AWR1243 for cascade design. We also looked at the published reference designs. The PDF file have two different parts, (i) AWR1243 and (ii) XWR1243.What is the difference in features between the two?

(2) The AWR  1243 Data sheet  (SWRS188 –MAY 2017) shows that cascade is supported in AWR1243, when compared to AWR1443 and AWR1642. However, we are told now that ARW1243P variant of AWR1243 only supports cascading options. Is that true? We have already ordered the part AWR1243 (Part No: AWR1243FBIGABLRQ1). Is there anything that can be done? We can switch to AWR1243P parts in future. What can be done with the ordered parts? Besides incurring extra money for the new order, our design time is also extended. If there is any software fix, for using these parts, that would be greatful.

Regards

Ganesan

  • Hi,

    Answer #1

    XWR1243 are pre-production devices that did not go through complete testing flow.

    AWR1243 are production devices that have gone through complete testing flow

    Answer #2

    Let me clarify this with extended team

    thank you

    Cesar

  • In reply to Cesar:

    Hi,

    I was communicated that AWR1243 ES 3.0 (production part) does not support cascade.

    Unfortunately there is no software workaround.

    Only AWR1243P supports cascade

    Thank you

    Cesar

  • In reply to Cesar:

    Hi Cesar:

    Thanks for your note.

    1.Does it mean that ES 2.0 samples of 1243 support cascade option? We would like to use the current samples if possible before we order the new parts of 1243P. Of course, for any future use, we will order 1243P.

    2. How do we find what we ordered are ES 3.0 samples not ES2.0 samples?

    Regards

    Ganesan

  • In reply to Ganesan Thiagarajan53:

    FYI, I have already mentioned the part number we ordered in my first mail.

    Regards

    Ganesan

  • In reply to Ganesan Thiagarajan53:

    SOrry for delay

    Please check the marking on silicon.

    If you see "ABL" it should be PG 3.0

    Thank you

    Cesar

    AWR1243

    IG

    87ZF9G9

    964FC ABL G1

  • In reply to Cesar:

    Hi Cesar:

    Thanks for your note.  You have answered one of my question.Since our part number has "ABL" in it (AWR1243FBIGABLRQ1), I assume they are 3.0 samples.

    Can you please confirm whether we can do the cascade with ES 2.0 samples? I will check our inventory.

    If we are lucky we can use those samples, since it will take more time for the 1243P samples to be procured from our side.

    Regards

    Ganesan

  • In reply to Ganesan Thiagarajan53:

    Yes,

    ES 2.0 samples support cascade using the Firmware version 1.0

    Thank you

    Cesar

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.