Other Parts Discussed in Thread: TFP401, TFP401A, TDA2HG, TFP410
Hi,
I am new to TI processors family, i have an application of DMD for which i am using 5530, below is the thread where some discussion has happened
My Requirement is to take HDMI input and do a Diamond preprocessing on a DSP and throw the processed output on HDMI output port
are there any TI processors which can taken HDMI input on one port and HDMI output on other port or 2 HDMI ports ?
because my input and output are continous, also here i may not use same port for both input and output
are there any design example which have done this ?
---------------------------------------------------
After further study i am adding a edit
I understood even the DLP Kits use a de serializer for HDMI to parallel conversion
so i can use a TFP401A to convert the incoming HDMI to processor input and do the processing and further throw the output data to TFP401
to do above i may need two video ports of 24bit, kindly suggest a processor which can do processing operations and throw the data over HDMI
do i need any Linux to use these processors ? i assume bare metal is much effiecinet kindly let me know which TDA family of processor is much better for DLP diamond preprocessing applications.