This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI Input and HDMI Ouput Processor or DSP

Other Parts Discussed in Thread: TFP401, TFP401A, TDA2HG, TFP410

Hi,

I am new to TI processors family, i have an application of DMD for which i am using 5530, below is the thread where some discussion has happened

DLP5530S-Q1: How to achieve 1:1 aspect ratio - DLP products forum - DLP®︎ products - TI E2E support forums

My Requirement is to take HDMI input and do a Diamond preprocessing on a DSP and throw the processed output on HDMI output port

are there any TI processors which can taken HDMI input on one port and HDMI output on other port or 2 HDMI ports ?

because my input and output are continous, also here i may not use same port for both input and output

are there any design example which have done this ?

---------------------------------------------------

After further study i am adding a edit 

I understood even the DLP Kits use a de serializer for HDMI to parallel conversion

so i can use a TFP401A to convert the incoming HDMI to processor input and do the processing and further throw the output data to TFP401

to do above i may need two video ports of 24bit, kindly suggest a processor which can do processing operations and throw the data over HDMI

do i need any Linux to use these processors ? i assume bare metal is much effiecinet kindly let me know which TDA family of processor is much better for DLP diamond preprocessing applications.