This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVCP22: Basic questions

Part Number: SN65LVCP22


Hi,

Let me ask you some basic questions as below.

Q1) unusued IN+/IN- pins

Will you tell me how to handle these pins in case unusing?

Is it possible to leave "open"?

Q2) EN0/EN1

In case of using these pins with "H" fixed, is it possible to connect 3.3V directly?

Because there are 400ohm and 300Kohm resisters at the input.

(Datasheet 3page, "equivalent input and output schematic diagrams") 

Q3) SEL0/SEL1

I would like to use both pins with "L" fixed.

In this case, I suppose we can connect both pins to GND directly according to the equivalent schematics.

Or is it possible to leave both pins "Open"?

Will you give me your advice?

Thank you for your support!

Best Regards,

Takumi

  • Takumi-san

    Q1) unusued IN+/IN- pins

    Will you tell me how to handle these pins in case unusing?

    Is it possible to leave "open"?

    For these unused differential inputs I would recommend to tie the "+" input to VCC and the "-" input to GND.

    Q2) EN0/EN1

    In case of using these pins with "H" fixed, is it possible to connect 3.3V directly?

    Because there are 400ohm and 300Kohm resisters at the input.

    (Datasheet 3page, "equivalent input and output schematic diagrams") 

    I would recommend connect to 3.3V through a 1k resistor.

    Q3) SEL0/SEL1

    I would like to use both pins with "L" fixed.

    In this case, I suppose we can connect both pins to GND directly according to the equivalent schematics.

    Or is it possible to leave both pins "Open"?

    I would recommend connect to GND directly.

    Thanks

    David

  • Hi David-san,

    Thank you for your reply !

    Let me confirm one point about Q2.

    Why do you recommend to use 1K resister?

    I suppose the reason that as there is "zener" diode in front of the input, 1K resister will guard from rush current.

    Is my idea correct?

    Thanks and Regards,

    Takumi

  • Takumi-san

    Correct, 1k will act as a current limiting resistor.

    Thanks

    David

  • David-san,

    Thank you very much for your reply !

    I understood.

    Regards,

    Takumi