Part Number: SN65LVCP22
Hi,
Let me ask you some basic questions as below.
Q1) unusued IN+/IN- pins
Will you tell me how to handle these pins in case unusing?
Is it possible to leave "open"?
Q2) EN0/EN1
In case of using these pins with "H" fixed, is it possible to connect 3.3V directly?
Because there are 400ohm and 300Kohm resisters at the input.
(Datasheet 3page, "equivalent input and output schematic diagrams")
Q3) SEL0/SEL1
I would like to use both pins with "L" fixed.
In this case, I suppose we can connect both pins to GND directly according to the equivalent schematics.
Or is it possible to leave both pins "Open"?
Will you give me your advice?
Thank you for your support!
Best Regards,
Takumi