Other Parts Discussed in Thread: USB2ANY,
Tool/software:
Dear TI experts,
I am testing TPS65235EVM-747 with USB2ANY interface board.
1. Installed TPS65235EVM GUI.
2. connect PC->USB2ANY->TPS65235EVM-747, and run EVM GUI.
3. I checked "not connected"(red dot) in the bottom left on the screen.

4. So I cannot control anything (reading registers, writing registers) in the GUI.

(Trying to write 1 to Bit 7 of 0x00)

(Trying to read status register)
5. After that I tried to update firmware using "USB2ANY Firmware Loader" and "USB2ANY Software Explorer" and restarted EVM GUI but I still can checked "Not connected" message in the bottom left.
Could you help me to connect PC -> USB2ANY -> TPS65235EVM-747? What is the wrong point?
And here are more questions;
1. I use the PC which OS is Windows 11, and my customer use the PC which OS is Windows 10. Could it be one of the problem?
2. I saw that "The Status for USB Adapter Connection only shows the status for the adapter, not the EVM board." -> So Is it the problem just between PC and USB2ANY? (not the problem of TPS65235EVM-747?)
Please check this issue. Thanks.