Other Parts Discussed in Thread: LMV772
Tool/software:
I am using the opamp LMV772.
I have non-Inverting negative feedback opamp configuration with gain is 11.
The opamp I/P is connected to a voltage divider and the application is voltage sensing
I am also using the second opamp in the IC as a buffer for another application, and there also the +ve input is connected to a resistor divide, to sense voltage.
Supply is single rail with GND as 0V and Supply as 5V.
In the datasheet the common mode voltage is mentioned as 0V to 4.1V. So this means I can only give a maximum of 4.1V to the non inverting terminal?