Other Parts Discussed in Thread: TIDA-00779, UCC27524, UCC27324, , UCC28070
Tool/software:
Hello,
I'm trying to understand what is causing Input Current Waveform distortion on 2 boards I have. They are both TIDA-00779 designs using the same PCB. Board#1 is an exact duplicate with the same Mosfet hardware and an output voltage of 390V / 3500W. (I'm using a slightly older PCB version from the most recent) Schematic is attached below.
Board #2 uses the same PCB but instead of mosfets, I'm using Infineon IKW40N120T2FKSA1 IGBTs. Instead of using UCC27324 drivers in Board#1, I'm using UCC27524 drivers in Board#2. Board#1 uses 12VCC, Board#2 uses 15VCC to drive the IGBTs. D1, D2, and D3 diodes in Board#2 are similar to the diodes used in Board#1 but are rated for higher voltage. Board#2 also uses a Capacitor array with the same capacitance rating to Board#1 but with a higher voltage rating.
Below are input Voltage and Current curves for Board#1 and Board#2. The blue line is voltage, yellow is current. Both voltage and current measurements were measured from a voltage divider and a 0.01R shunt resistor signals passing through isolation amplifier circuits.
Board#1 @ 1500W - Resistive Load
Board#2 @ 1500W - Resistive Load
My intention was to trial running higher output voltages on Board#2 to around 650VDC but I'm noticing input current distortion issues even at 390VDC output voltages. Both Board#1 and Board#2 exhibit the same distortion but it is much more pronounced in Board#2 than Board#1. I would like to resolve the distortion issue before I continue testing at higher output voltages.
Regards,