Part Number: OPA615
Other Parts Discussed in Thread: BUF602
Hi,
I my application, I would like to detect the moment when a cutting tool touches a grounded part. This during cutting so depending on the cutting speed, the signal is very short. My first try was to use a NAND RS-latch with Schmidt triggers. The tool is connected with 1k pull-up resistor to 5V.
But tests show this is not fast enough Then I came accross the datasheet of OPA615. Figure 48 shows something which I think comes close to what I need, but I'm not sure. This circuit should detect positive and negative pulses, but I assume negative here means lower then zero. I need the lowest positive value.
So, could somebody tell me if this circuit could be used to hold a 'positive valley', and if not how it can be adapted please?
Thanks in advance,
Best regards,
Marc
edit: picture added