Part Number: OPA615
Hello,
As referred to this thread I have small doubts in my application. My sensor output is in range of 20mV to 150mV with 5.9 MHz burst wave(delay1ms between next cycle). Because of low voltage, I have amplified it with Gain factor 50 and I want to measure the peak to peak of my output. Will this OPA615 be able to detect a peak of burst wave also? I have attached the image of my sensor output. I have attached the schematic that I have simulated with the continuous sine wave (f=6MHz). In my simulation, how can I precisely detect the peak? I mean the selection of diode and capacitance value. The output of OPA615 goes to my Arduino Uno for detection of voltage and further processing.
How can I simulate OPA615 with Burst signal in TINA? I have already tried with peak detector circuit using LTC5507 from Analog Device but it didn't give prominent output. And It is only worked with the continuous sine wave, not for burst wave. Can anyone give some guidance about that?OPA615_PeakDetector with amplifier.TSC