Part Number: TL026
Other Parts Discussed in Thread: TL082
Hello,
I am currently working on a infrared receiver and the problem is that the amplitude of the received AC Signal is changing in correspondence to the distance between the transmitter and receiver.
The received ac signal has a frequency of 40kHZ and the Peak-to-Peak Voltage ranges from 10mV to 40mV according to the distance. I have a supply voltage of +/-3.3V.
Is the TL026 capable of providing a constant Output Voltage of 700mV to 1000mV with the given AC Signal in spite of the changing distance issue?
Will the Circuit with no Attentuation (Fig.6) which is given in the datasheet work in my case?
Thanks
Dmitrij