Part Number: TPS25750
I want to replace a Barrel Jack connector with a USB-C PD port. The USB-C PD port only needs to Sink power. How can I optimize the schematic with the TPS25750 to achieve this functionality?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25750
I want to replace a Barrel Jack connector with a USB-C PD port. The USB-C PD port only needs to Sink power. How can I optimize the schematic with the TPS25750 to achieve this functionality?
Below is a block diagram with the minimum set passive components to implement a UFP (Sink) using the TPS25750D

| Passive Components | |
| Name | Value |
| C1 | 47uF, 25V |
| C2 | 10uF, 6.3V |
| C3 | 10uF, 6.3V |
| C4 | 10uF, 4V |
| C5 | 4.7uF, 25V |
| C6 | 330pf, 25V |
| C7 | 330pf, 25V |
| R1 | DNI |
| R2 | 0 Ω |
| R3 | DNI |
| R4 | 0 Ω |
| R5 | 2.2 kΩ |
| R6 | 2.2 kΩ |
| R7 | 10 kΩ |
| R8 | 2.2 kΩ |
| R9 | 2.2 kΩ |
| R10 | 10 kΩ |
Design Consideration Checklist:
Please refer to section 12 Layout on page 55 of the TPS25750 USB Type-C and USB PD Controller with Integrated Power Switches datasheet (Rev. A) for a representative schematic and layout recommendations.