This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM64X/AM62X: How do I route the same GPIO bank interrupts to different destination cores?

Part Number: AM6442


How do I route the same GPIO bank interrupts to different destination cores?

Example: I want to route the GPIO0_37 pin interrupt to R5F0_0 and the GPIO0_38 pin interrupt to R5F0_1.

when I was selecting the above pin combination from the system configuration and generated code. Then I noticed the below SCI client error when I was Running examples on R5F cores. then How can I solve this problem?

[MAIN_Cortex_R5_0_1] [Error] Sciclient event config failed!
ASSERT: 0.2338s: syscfg/ti_drivers_config.c:Sciclient_gpioIrqSet:116: FALSE failed!