Other Parts Discussed in Thread: BQ25186 , BQ21088 , BQ25180 , BQ25188 , BQ25185 , BQ21080 BQ2518x FAQ Home Page
This home page is for common questions in relation to the BQ25188, BQ21088, BQ25185, BQ25186, BQ25180, and BQ21088.
FAQs
----…
Part Number: AM62A7-Q1
Hi,
I am trying to do CPU reset for C7x core on AM62Ax device and facing a page fault error.
Below is the error message.
"(Error -1351 - (0:0:0)) Register or Memory request has timed out. The CPU is executing a High Priority…
Part Number: AM62D-Q1
When implementing audio input/output systems using MCASP (Multichannel Audio Serial Port), there is inherent latency in the audio pipeline(SW) due to buffer priming and the DMA queuing mechanism. This FAQ explains the fundamental…
Part Number: AM62D-Q1
By default, The AWE SDK uses the AWE Designer to load any signal processing chain. However, once the signal chain is finalised, how to load the signal chain on startup without the use of AWE Designer?
Part Number: TMP103
Hello Team,
Regarding the TMP sensor family, are they able to run at 100kHz as named ‘Standard Mode’ in the I2C standard? If so, are all the sensor specifications compatible with the I2C standard?
Part Number: TMS320F2800137 Other Parts Discussed in Thread: C2000WARE
Hello,
I want to port the E-Metrology library fom F28P55 to F2800137. I want to enable only single-phase calculations and I do not wish to calculate THD. What steps can I follow…
Other Parts Discussed in Thread: AM2431 Hello Randy
AM2431: MCU design: PCIe differential impedance value
Since the 2 queries are 2 different topics, i will split the thread.
For PCIe interface traces impedance control, I get different information…
Part Number: BQ25188 Other Parts Discussed in Thread: BQ25185
TS pin operation
The BQ2518x uses an internal 38uA current source on the TS pin to bias the NTC thermistor, and the resulting TS voltage is compared against internal reference voltage thresholds…
Part Number: AM620-Q1
There are more than 30 ECC aggregators in each of AM62x, AM62Ax, AM62Px and AM62Dx devices. How do we find the ESM events corresponding to each of the ECC Aggregators?