Part Number: AM625
The new Boots Quirk Function, Flash_quirkSpansionSafebootDetection , introduced in MCU+ SDK 11.02, is specifically designed for Serial NOR Flash devices (S28HS512T and S25HL512T). If you are using custom Flash parts, you must modify…
Part Number: TDA4VH-Q1
When a user presses Ctrl-C to stop the application, the default behavior sets a shutdown flag but may not perform proper cleanup. The main application thread could be blocked waiting for messages from the remote cores (R5F, C7x…
FAQ: Logic and Voltage Translation > > Current FAQ
[FAQ] What is the Difference Between I2C and SPI I/O Expansion
[FAQ] VOH/IOH/VOL/IOL and Total ICC Current Definitions
Other Parts Discussed in Thread: TMDX654IDKEVM I want to test PRU Ethernet on the AM65x IDK EVM (TMDX654IDKEVM).
I am using Linux SDK 11.2. I am booting the default filesystem image, tisdk-default-image-rt-am65xx-evm-11.02.05.02.rootfs.wic.xz. However…
Part Number: CC2745R10-Q1 Other Parts Discussed in Thread: CC2755R10
This post presents three example projects demonstrating incremental BLE functionality on the TI CC2755 microcontroller using Zephyr 3.7.0 v3.7.0-ti-9.14.00_ea.
All projects use:…
Part Number: J784S4XEVM Other Parts Discussed in Thread: DRA821 , TDA4VL , AM68 , TDA4VM , TDA4VH
How do I troubleshoot the McSPI interface within Linux? McSPI is not working or partially working.
Part Number: AM62A7
Q: The default memory map for AM62A does not work for my application. How do I modify the RAM / DDR memory map to suit my module size and application?
Part Number: TPS546E25
Which version of FUSION GUI supports TPS546E25 and where to get it?
TI FUSION Digital Power Designer 7.10.5 and later supports TPS546E25
Version 7.10.17 is available here Link to Product Folder
note on versions 7…