Snubber circuits are designed to suppress voltage spikes, limit the rate of voltage and current changes, and protect switching devices from damage.
It is recommended to use snubber circuits across SW and Vin, and across Flyback diode. Refer this technical…
Part Number: LM5180-Q1
Flyback transformer
To operate as flyback converter, transformer polarity has to be as expected, reversing polarity makes the converter work as forward converter which cannot provide expected output when loaded. Also, check…
RSET resistor is used to set the internal 1.21-V reference to the input of the error amplifier for internal closed loop. RSET is recommended to keep at 12.1 Kohm to maintain 100uA current in RFB and RSET resistors, and vary RFB to obtain required output…
Select a Schottky diode for this application to account for inevitable diode voltage overshoot and ringing related to the resonance of transformer leakage inductance and diode parasitic capacitance. Connect an appropriate RC snubber circuit (for example…
Other Parts Discussed in Thread: LM25184 Connect a diode-Zener clamp circuit across the primary winding to limit the peak switch voltage after MOSFET turnoff.
We recommend using a Zener diode with a clamp voltage of ~1.5x the reflected output voltage…
Other Parts Discussed in Thread: LM25180 , LM5180 , LM25185 , LM25184 , LM25183 , LM5185 , LM5181 LM5180/1, LM25180/3/4 FAQs Home Page
This home page is for common questions in relation to the LM5180, LM5181, LM25180, LM25183, LM25184, LM25185, LM5185…
Part Number: AM625
- SYSFW/TIFS Crypto Service The crypto services allow SYSFW/TIFS client to encrypt/decrypt data blobs using one of AES-ECB, AES-CBC or AES-GCM operations. - SYSFW/TIFS Crypto Service API https://software-dl.ti.com/tisci/esd/latest…
Part Number: TPS25751A Other Parts Discussed in Thread: TPS26750 , TPS25751 , , TPS26750A , BQ25713 , BQ25731 , BQ25756 , BQ25756E , BQ25690
What are the differences between the A and non-A versions?
Feature
TPS25751/TPS26750
TPS25751A/TPS26750A…
Part Number: TPS25730A Other Parts Discussed in Thread: TPS25730
What is the TPS25730A?
The TPS25730A is a stand-alone USB Type-C and Power Delivery controller optimized for applications supporting USB-C PD Power Sink-only applications.
Why…