Part Number: J784S4XEVM
Hi Team, How can the performance of a custom kernel be benchmarked using GTC Timer and TSC, and how can the results be evaluated across different optimization levels?
Part Number: AM13E23019
Hi ,
When trying to connect am13x launchpad we get the following errors;
CS_DAP_0: Error connecting to the target: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target…
Part Number: AM62xx Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG
How can flashing speed be improved in UART Uniflash using a higher baud rate?
Overview Flashing speed using UART Uniflash on the AM62XX platform can be partially improved. A…
Part Number: MCF8316D Other Parts Discussed in Thread: DRV10983 , DRV10975 , DRV10987 , , MCF8316A
TI pioneered the industry’s first fully integrated motor‑control driver that requires no external code for configuration, delivers faster…
Part Number: AM625 Other Parts Discussed in Thread: AM62P , AM62L
Overview
This article describes how to build and boot DFU enabled U-boot images on TI-K3 devices such as AM62X, AM62A AM62P, AM62L and AM64L using Yocto
USB-DFU (Device Firmware Upgrade…
Part Number: LOG200
Hi All,
I have a question regarding the LOG200.
The output is oscillating on a customer's circuit board, and I am seeking your assistance.
The circuit board situation is as follows: A PD in a completely dark state is connected…
Part Number: AM2434
On HSSE devices, the SYSFW supports the Keyring feature which extends the Root of Trust ( RoT ) to auxiliary keys. This enables the authentication of the application images using these auxiliary keys apart from the programmed SMPKH…