Part Number: BQ25756 Other Parts Discussed in Thread: BQ25750
There are 4 registers for the BQ2575X family that control reverse mode, EN_REV, VAC_REV, IAC_REV, and SYSREV_UV. For the BQ25750 specifically, these registers are EN_REV, VSYS_REV, IAC_REV…
Part Number: BQ25756
Hello, For the BQ2575X family, 80µF is the minimum after derating for the input and output capacitance. 160µF of input and output capacitance is based on meeting a ±3% transient response requirement. Keep in mind, you'll also need…
Part Number: BQ25758 Other Parts Discussed in Thread: BQSTUDIO
Hello,
Here is a link to the BQ25758 BQZ file: Charger_2_00-bq25758.bqz
To install this bqz file, download the file and move it to the config folder of the BQStudio installation. Best…
Part Number: BQ25750 Other Parts Discussed in Thread: BQSTUDIO
Hello,
Here is a link to the BQ25750 BQZ file: Charger_2_00-bq25750.bqz
To install this bqz file, download the file and move it to the config folder of the BQStudio installation. Best…
Part Number: LMH1297
When signal goes through two different transmission line, signal may get reflected based on difference between these two medias impedances. Return loss is the ratio of the reflected signal to the launched signal. If signal goes…
Part Number: AM6442
Hello,
I am trying to understand what voltage levels I am looking at with the AM6442 SERDES driver. I am using the IBIS-AMI model in HYPERLYNX I am seeing the common mode output voltage swing from 200 to 600 mV with a centerpoint…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62B ,
Overview
In some applications it is critical that SPI transfers happen with the smallest-possible inter-byte gaps to either optimize throughout, or to meet certain overall system real…
Part Number: TUSB522P Other Parts Discussed in Thread: TUSB1002A , TUSB1044 , TUSB542 Hi Experts,
I see parts like the TUSB1002A and 1044 described as "linear" re-drivers while the TUSB522P is a "limited" re-driver. Which one is better to use in a USB…
Part Number: TUSB1002A Other Parts Discussed in Thread: TUSB1064 , TUSB1044
Hi Experts,
Will the TUSB1002A recover the loss before or after the re-driver?
Best,
Shane
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 , , SK-AM62B
Overview
It is a common need wanting to incorporate a custom Linux device tree file into the boot process of Yocto-generated filesystem images. This FAQ introduces a simple and…